Advanced Reporting and Dashboards component

Advanced Reporting and Dashboards Module is a variant of Power Monitoring Expert (PME) that is included on the Power Operation installation media and can be optionally licensed with Power Operation. In an architecture with Power Operation, the Reports and Dashboards components of Power Monitoring Expert(PME) are integrated with the Power Operation Runtime to deliver a feature-rich “Energy Monitoring Application” experience for the system. Additionally, WebReach diagrams are commonly integrated into the Power Operation Runtime as well.

Topics in this section: