Server component architecture

Built-in architectural redundancy

Power Operation supports full server redundancy and full communication redundancy. When the Primary Server becomes unavailable, the Standby Server automatically takes over in 2 to 3 seconds.

There is also full data synchronization between servers and historical backfill. If primary goes down and a secondary becomes active, when the primary returns to active state the secondary fills in the primary with any missed information.

NOTE: Multiple NICs are supported on each server and a device may have two communication paths.

Making changes while online

Certain changes and updates to a production Power Operation system require a restart of the Power Operation Server processes. For example:

  • Adding and removing devices
  • Adding and removing tags

For this reason, if the customer requires changes to be made without interruption of service (restarting Power Operation Server), a redundant architecture is required.

In a redundant architecture, changes can be made without interrupting service by:

  1. Making a change on Secondary Server
  2. Restarting Secondary Server
  3. Making the updated Secondary Server the Primary Server

Ethernet network redundancy

When network redundancy is being considered, the most common approach is: Second LAN in parallel to first. If LAN1 becomes inoperative, components will maintain connection using LAN2.