Connected devices and protocols
Power Operation supports concurrent protocol communication; one Power Operation server can communicate using multiple protocols.
Power Operation 2022 supports the following protocols:
- IEC 61850 Primary (sometimes called Master) Edition 2
- DNP3 Primary
- ION
- Modbus Primary
- IEC 60870-5-104 Primary
- KNX
- SNMP
- BACnet/IP
Power Operation supports the following Open Data Exchanges:
- OPC UA 1.01 (Client and Server)
- OPC DA version 2, version 2.05a (Client and Server)
- OPC AE version 1 (Server)
Go to the AVEVA Knowledge & Support Center website for information on Plant SCADA.