Smart Connector Overview

Smart Connector unlocks data sharing with systems in which Power Operation does not already have built-in communication support. Smart Connector is an open, extensible, and documented application framework that simplifies integrations with third-party systems or data sources.

Using the Smart Connector development kit, software developers can create extensions to share Power Operation real time and alarm data with other systems.

Options for Smart Connector extension development
  • Have Schneider Electric do it for you: Those without software development capabilities can contact the Digital Energy Center of Excellence to quote potential projects.

  • Do it yourself: Customers, EcoXperts, and Digital Power Application Centers with software development capabilities can download the Developers Guide for Smart Connector. Go to the Schneider Electric Exchange for more information.

Smart Connector development overview
  1. Learn about Smart Connector.
  2. Develop extensions via .NET.
  3. Install and Deploy Smart Connector Framework/Runtime and custom extension.