Web Client versus Thick Client
The HTML5 Web client and Thick client both have unique graphics engines. Legacy graphics pages built using 'classic' graphics builder will only run in the Windows Thick client application. Conversely, Web client graphics with pan/zoom capabilities will only run using a web browser.
A single Power Operation Server can provide both a Windows runtime experience and an HTML5 web client operator experience. However, graphics cannot be reused between the Windows Thick client and HTML5 Web client.
| Windows Thick client runtime options | HTML5 Web client |
|---|---|
| Operator access via Windows application: | Remote operator access via web browser: |
|
|
|
|
|
|
|
Web Client versus Thick Client feature comparison
| Feature | Thick client capability | HTML5 Web client capability |
|---|---|---|
| Graphics monitoring only | Yes | Yes (plus pan/zoom scalable graphics and decluttering) |
| Alarms | Yes | Yes (plus Smart Alarm grouping, timeline analysis, natural language waveform analysis, shelving, disabling) |
| Waveforms | Yes | Yes (plus waveform comparison) |
| Alarm banner annunciator with audible alarms | Yes | Yes (plus ability to navigate to alarm views and ability for end users to configure |
| Ability to navigate from graphic to associated alarms | Yes | Yes |
| Client side scripting | Yes (using CiCode) | Yes (using JavaScript) |
| Graphics monitoring and control | Yes | Yes |
| Trend viewer (real time and historical) | Yes | Yes |
| Runtime container customization | Yes | Partial (plus ability for end users to configure) |
| Ability for local teams to translate end user runtime | Yes | No (various languages available with EPO 2021) |
| Two-factor authentication support | Yes | No |
| Role-based access control of various web components | Yes | No |
| Client automatically switching to secondary server during failover | Yes | No |
| Configuration/tools: ENM configuration (functionality introduced in PSO 9.0) | Yes | No (end users using web client as primary interface can use thick client runtime to use ENM configuration) |
| Configuration/tools: Tag Viewer and Tag Debugger (functionality typically used by engineers or tech support for diagnostics/troubleshooting) | Yes | Partial (end users using web client as primary interface can use thick client runtime to use Tag Viewer/Debugger) |
| Configuration/tools: Scheduler configuration | Yes | No (Note: End users using web client as primary interface could use thick client runtime to use the Scheduler configuration/application tool.) |
HTML5 Web client browser support
|
|
Google Chrome |
Mozilla Firefox |
Apple Safari | Microsoft Edge |
|---|---|---|---|---|
| Power Operation graphics pages including one-line diagram/engine using pan/zoom graphics | Yes | Yes | Yes | Yes |
| PO 2021 Alarms and Trends | Yes | Yes | Yes | Yes |
| PME reports and dashboards | Yes | Yes | Yes | Yes |
| Power Operation Basic Reports | Yes | Yes | Yes | Yes |
| LiveView (Power Operation Real Time Tables implementation) | Yes | Yes | Yes | Yes |
NOTE: Graphics pages built using classic graphics builder will only run on Windows Desktop clients.