Backing up a Power Operation system
This section includes the tasks required to create automated backups of a Power Operation system. It also lists the installation media you need to back up, and the steps you should complete to prepare for the backup process.
NOTE: Some procedures in this section cite scripts you can use to automate the backup and restore process. Refer to www.se.com or the Schneider Electric Community for the backup and restore scripts specific to your Power Operation system version.