Power Monitoring Expert config folder
To reproduce the system in the case of a catastrophic failure, a copy of the \config folder should be stored in an off PME server location. This holds all the files that make your PME system unique. The copy of the \config folder only needs to be done once unless subsequent changes are made to the system.