Power Monitoring Expert diagnostics
Run a diagnostic capture using the Diagnostics Tool available in PME. Doing so stores information about the source PME system—including server specifications and OS/SQL versions—that are necessary to rebuild the system. Store the resulting .cab file in the off PME server location.