Verify notifications

On a newly installed Power Operation server:

  1. Create, compile, and run a simple project.
  2. Open the Notification Settings. See Creating Notifications.
  3. Add at least one recipient.
  4. Add the settings for at least one delivery method. See Configure SMS Text Notification or Configure the Email Server.
  5. Use the Test button to send a test message to the recipient. See Enable and Test Delivery.