Uninstall and reinstall Power Operation
Use Add/Remove Programs in the Windows Control Panel to uninstall these programs:
- Power Operation v2022 (if you uninstall this, you also uninstall the Profile Editor)
- Power Operation Profile Editor
- Graphics Editor
- Any additional Power Operation programs, such as the WebServer, that you installed
If you uninstall programs after you have already created projects, the project data will not be deleted. It is in [Project Drive]\ProgramData\Schneider Electric\Power Operation\v2022\User. The first time you open the application after you re-install it, it will locate the project data and re-link it.
Uninstall does not remove all files from the system. Decommissioning removes Power Operation files from your system to prevent potential disclosure of sensitive, confidential, and proprietary data and software from your Power Operation system. You risk disclosing your power system data, system configuration, user information, and passwords if you don’t decommission. We strongly recommend you decommission your system at the end of its' life.