Configuring a Distributed Database
Power Operation can connect to a remote PostgreSQL database or to a local instance of PostgreSQL database that has not been installed by EPO. For a successful connection to the remote/local instance of PostgreSQL database, confirm the following setup tasks are completed prior to installation of EPO. If the local instance of the PostgreSQL database has been installed by a previous version of EPO, then no additional setup tasks are required. Contact the Schneider Electric Support team if you need support with PostgreSQL installation on your remote computer.
NOTE: It is recommended that you uncheck the pg_admin option during the manual installation of PostgreSQL database.
Prerequisites:
- PostgreSQL is installed and running on the remote machine.
- Confirm PostgreSQL is running on port 5432.
- You have the PostgreSQL superuser credentials and password.
To configure PostgreSQL distributed database:
To configure PostgreSQL distributed database on Microsoft Windows:
- Copy and save the following scripts from the install ISO path
...:\Power Operation\Setup\Setup Support\PostgreSQL- create_default_po_user.sql
- po_db_schema.sql
- set_po_user_db_access.sql
- Open the
create_default_po_user.sqlscript, update the password, and save the file.NOTE: The password saved in this file is the same password that you need to enter for the User Name po_data during EPO installation.
- Run the following commands from the postgresql bin directory:
psql -U postgres -c "REVOKE CREATE ON SCHEMA public FROM PUBLIC; - Run the following command from the postgresql bin directory:
psql -U postgres -f ...\Users\<User ID>\<folder>\Scripts\create_default_po_user.sql. - Run the following command from the postgresql bin directory:
echo SELECT 'CREATE DATABASE po_scadadb' WHERE NOT EXISTS (SELECT FROM pg_database WHERE datname = 'po_scadadb'); \gexec | "...\Program Files\PostgreSQL\14\bin\psql.exe" -U postgres - Run the following command from the postgresql bin directory:
psql -U postgres -d po_scadadb -f "...\Users\<User ID>\<folder>\Scripts\set_po_user_db_access.sql" - Run the following command from the postgresql bin directory:
psql -U postgres -d po_scadadb -c "CALL set_po_user_db_access('po_data', 'po_data_role'); DROP PROCEDURE IF EXISTS set_po_user_db_access(text, text);" - Run the following command from the postgresql bin directory:
psql -U postgres -d po_scadadb -f "...\Users\<User ID>\<folder>\Scripts\po_db_schema.sql"
To configure PostgreSQL distributed database on Linux machine:
- Copy and save the following scripts from the install ISO path
...:\Power Operation\Setup\Setup Support\PostgreSQL- create_default_po_user.sql
- po_db_schema.sql
- set_po_user_db_access.sql
- Open the
create_default_po_user.sqlscript, update the password, and save the file.NOTE: The password saved in this file is the same password that you need to enter for the User Name po_data during EPO installation.
- Run the following commands from the postgresql bin directory:
psql -U postgres -c "REVOKE CREATE ON SCHEMA public FROM PUBLIC; - Run the following command from the postgresql bin directory:
psql -U postgres -f "...\Users\<User ID>\<folder>\Scripts\create_default_po_user.sql". - Run the following command from the postgresql bin directory:
CREATE DATABASE po_scadadb -U postgres - Run the following command from the postgresql bin directory:
psql -U postgres -d po_scadadb -f "...\Users\<User ID>\<folder>\Scripts\set_po_user_db_access.sql" - Run the following command from the postgresql bin directory:
psql -U postgres -d po_scadadb -c "CALL set_po_user_db_access('po_data', 'po_data_role'); DROP PROCEDURE IF EXISTS set_po_user_db_access(text, text);" - Run the following command from the postgresql bin directory:
psql -U postgres -d po_scadadb -f "...\Users\<User ID>\<folder>\Scripts\po_db_schema.sql"