Migration Tools
The automatic update that occurs when you initially open Power Operation 2022 does not fully upgrade your projects, and needs to be followed by using the Migration Tools. If you are migrating from v7.x, this is particularly noteworthy. The automatic update is a passive action which updates the database field definition for any database that has been changed between the two versions and copies new files that are necessary in 2022.
There are two main migration tools: one for Plant SCADA and one for Power Operation. Both must be run manually after the automatic upgrade has been executed. You can do this after you have prepared the project for final migration.
warning
UPGRADE ALTERS communications configurations
After upgrading, confirm and adjust the configuration of I/O devices in your project.
Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.