Version Information
To identify the version of Power Operation installed:
- Open Power Operation > Power Operation Studio.
- Select the program icon on the top left:

- Select About EcoStruxure Power Operation > Technical Info tab.
| Power Operation version | Plant SCADA file version |
|---|---|
| PO 2022 | 8.4 |
| PO 2021 R1 | 8.3 |
| PSO 2020 R2 | 8.21 |
| PSO 2020 | 8.2 |
| PSO 9.0 | 8.10.0.2086 |
| PSE 8.2 | 8.0.0.2065 |
| PSE 8.1 | 7.50.0.4150 |
| PSE 8.0 SR1 | 7.50.0.4107 |
| PSE 8.0 | 7.40.1.239 |
| PSE 7.40 SR1 | 7.40.1.239 |
| PSE 7.40 | 7.40.1.239 |
| PSE 7.30 SR1 | 7.30.0.601, 7.30.1.94 |
| PSE 7.20 SR1 | 7.20.4.38 |
| PSE 7.20 | 7.20.1.33 |