Create composite device profiles
A composite device profile includes more than one device type. Each device type can use its own protocol for communication.
With the composite device type, the user can use two devices for a single monitoring point. For example, a circuit breaker and a monitoring device can provide data to this single point. Because Power Operation combines the functionality of the multiple devices, end users only need to consider a single device when analyzing a location in their system.
The following links provide instructions for specific device types:
- Creating a third party Modbus Device Type
- Creating a composite device type
- Creating a data concentrator
- Setting up a G3200 gateway