Automatic transfer switch (ATS) information

ATS Information

The most commonly used information about the ATS genie displays by default.

When the Advanced Properties box is selected, the table expands to include everything that is known about the selected ATS.

Basic ATS information includes:

Column

Description

State

Normal (), Warnings (), or Errors (). See the following table for explanations of errors.

Page

Name of the page on which the genie is found (displays only from the folder level).

ID

This is the breaker number for the left side, assigned when adding it to a page of a one-line.

ID2

This is the breaker number for the right side, assigned when adding it to a page of a one-line.

Source Busbar1

The number of the source busbar for the left side.

Source Busbar2

The number of the source busbar for the right side.

Dest. Busbar

The number of the destination busbar.

ATS Errors

Before you use the drawing, correct all errors; otherwise the project might not compile and the animation will not work.

Errors that you might see for ATSs are:

State

Solution

Errors ()

Breaker numbers must be a number greater than 0 and unique.

The breaker numbers are missing, or they are less than or equal to 0. Add or change the breaker numbers.

Source busbar numbers must be a number greater than 0.

The source busbar numbers are missing, or they are less than or equal to 0. Add or change the source busbar numbers.

Destination busbar number must be a number greater than 0.

The destination busbar number is missing, or it is less than or equal to 0. Add or change the destination busbar number.

Source and Destination busbars must not be equal.

The source and destination busbars have the same number; change one number.

Either the Source or Destination Busbar number must exist (busbar may link to a Busbar, transformer, meter, source, or another breaker)

At least one busbar must be linked to this ATS.