Create a LiveView template

To begin creating LiveView templates:

  1. In Programs, click Schneider Electric Table Editor.
  2. The LiveView Template Editor screen displays.

  3. Open LiveView Template Editor click New.
  4. An empty template displays with a "New Template" name.

  5. In Template Name, enter the template name. You can use up to 100 characters; limited to A–Z, a–z, 0–9, spaces, underscores, hyphens, and parentheses.
  6. In Single Device/Multiple Devices, keep the default single device or click Multiple Devices.
  7. To continue setting up the template, click one of the following links:

NOTE:  Table grid lines do not display in the LiveView Viewer, however, they do display in LiveView Setup.