LiveView delete
You can delete any template except one that is predefined.
- Open LiveView Template Editor.
- In Power Operation Runtime, click the menu links that have been set up when you created the graphics page (see Create menu item for LiveView page). In the PLS_Example project, there is a tab for LiveView.
- Highlight the name of the template that you want to delete. The template displays.
- Click Delete (on the top of the left-hand pane).
- You are prompted to verify the deletion.
- Click Yes to delete the template, or click No to cancel the deletion.
- Continue working with other templates.