Configuring an automatic transfer switch (ATS)
To configure an automatic transfer switch (ATS) you have added to a one-line in the Graphics Editor:
- Edit the following properties:
- Exposed Properties:
CommonBusName, MainBusName, and AuxBusName
Set to the busbar component name that represents the buses to which the ATS is connected. - Binding Conditions:
PosOnEmergencyCond and PosOnUtilityCond
You can leave these empty if your equipment has an item name (AtsSwMainCls or AtsSwAuxCls) set for the variable tag. You can also set the condition using a variable tag by creating a Boolean expression for the position of the ATS.
- Exposed Properties:
This component helps establish the connectivity by which the advanced one-line will energize buses based on connected sources.
If an ATS is configured incorrectly, use the Connection Debugger to troubleshoot the following:
- Ensure the CommonBusName, MainBusName, and AuxBusName are set.
- Ensure the conditions have valid Boolean expressions. For more information, see Condition attribute expressions.