Create Device Profiles
Use the Create Device Profiles screens to view and edit profiles for individual devices. Profiles are predefined for standard devices; you will mostly use this feature to add third-party device profiles.
After device types are added to the project, use the Create Device Profiles windows to view and edit profiles for individual devices. Because profiles are defined for standard devices, use this feature to add third-party device profiles. On these windows, you can make changes to a standard device type, and then save the device as a profile that is included in your project.
Before you create profiles, you need to be sure that all of the tags and device types that you need are created (see Define Device Type Tags). Also make sure that you have added any new units or conversions and device type categories and subcategories that are needed.