Define multiple devices using a CSV file

I/O Device Manager makes it easy to create a Power Operation project. Use this tool to make either single or bulk additions, updates, and deletions to the Power Operation device database.

Valid communication protocols are:

  • DNP3 Serial
  • DNP3 Ethernet
  • Modbus/RTU Gateway
  • Modbus TCP
  • ION
  • ION/Gateway
  • IEC60870-5-104 TCP
  • IEC61850

Topics in this section: