Add project parameters

The Project Parameters sub-tab allows you to add optional lines of information about this project. This information can be used for verification or identification when you want to import the project.

To add project parameters:

  1. From the Set Up Projects tab, select the Project Parameters sub-tab.
  2. On the first available line, type a name and value for this information. Example: If you want to track versions, in the Name field, you might type "Version." Then, in the Value field, type the appropriate version for this project.

The new parameter is added. It will help you identify the project when you want to import it into another instance of the Profile Editor.