Moving files when the Profile Editor is not on the server
If the Profile Editor is not on the same computer as the Power Operation server, you need to move the export file to the server computer.
To move the export file to a different server:
- Export the project from the Profile Editor:
- Select the folder icon beside the Export Project button link:

- Copy the file Equipment.profiles that displays and move it to a portable drive.
- Select the folder icon beside the Export Project button link:
- On the Power Operation server computer, paste Equipment.profiles to the following location:
- Use I/O Device Manager to begin adding device information to the Power Operation project.
[Drive Letter]:\Documents and Settings\All Users\Application Data\Schneider Electric\Power Operation v2022\User\[Project]
Where:
[Drive Letter]: The the drive on which you installed the Power Operation server
the Application Data and ProgramData folders cannot be hidden (set the folder view for “view hidden folders”)
[Project]: The name of the project you are creating; you must have already added this project to Power Operation (see Before you export a project).