Compile the project

In Power Operation Studio, click Compile . If you are promoted to save your changes, click Save.

If there are errors or warnings after the project is compiled:

  1. At each error, click GoTo, which opens the location where the error occurred.
  2. Using the information in the error message, correct the error.
  3. After all errors are addressed, re-compile to verify that the errors are removed.

    For additional information, click Help at the error screen.