Restoring a project

Restore a project from a backup and overwrite its current settings.

After restoring a project:

  • Update restored TGML files using the TGML Upgrade Utility. See TGML Upgrade Utility for detailed steps.

  • Update Graphics Editor components using the EcoStruxture Power Operation 2021 R2.1 Migration Tool. See Using the Migration Utility for detailed steps.

Restore a project

  1. Open Power Operation Studio.
  2. Click Projects .
  3. Click the Backup drop down and then click Restore.
  4. Beside the Backup file text field, click Browse, and then browse to the location of the project file you will use to restore.
  5. (Optional) Click Select all included projects, with the exception of the PLS_include project.
  6. In the To area, click Current Project.
  7. In the Options area:
    1. Click Configuration files to restore backed up INI files and the TimeSyncConfig.xml file (used to store time synchronization settings).
    2. If you backed up the sub-directories under the project, the directories will be listed under Select all sub-directories to restore. You can restore all or no sub-directories, or you can select specific sub-directories to restore.
  8. Click OK.