System startup and validation checks

To test and validate the project:

  1. Test two-factor authentication. For more information, see Log in with YubiKey.
  2. Test the Web Client: Open the Web Client and verify that links are working properly.
  3. Test the advanced one-line.
  4. Test single sign-on to Dashboards, Advanced Reports, and Web Diagrams.
  5. Verify that I/O Devices are Communicating.