Configuring a source

To configure a source you have added to a one-line in the Graphics Editor:

  1. Edit the following properties:
    1. Exposed Properties:
      ActiveColor
      Set to the color you want all connected busbars to display when the source is energized.
      BusName
      Set to the busbar component name that represents the bus the source is feeding.
    2. Binding Conditions:
      ActiveCondition
      Using a variable tag, create a Boolean expression for whether or not the source is energized.

The advanced one-line will color all of the busbars connected to this source based on the active condition and active color set above.

If a source is configured incorrectly, use the Connection Debugger to troubleshoot the following: