Add single single sign-on settings to Citect.ini
Use this procedure to add the single sign-on properties of Advanced Reporting and Dashboards Module.
To add single sign-on settings to Citect.ini:
- Open the Citect.ini file (typically in
C:\ProgramData\Schneider Electric\Power Operation\v2022\Config). In this file, you will add the following SSO values (if they are not already there): - Complete each parameter with the value specified below. Then save the modified citect.ini file:
[Applications] Hostname= WebReachServer= Area= PrivLevel= UseHTTPS= PSEHostname=
Hostname– The name or IP address of the computer that hosts Advanced Reports and Dashboards (Power Monitoring Expert).WebReachServer– Default value: empty string. This parameter specifies the host name or IP address of the WebReach server machine. In most cases this is the same as theHostnameprevious. Required for integration with WebReach to display Diagrams in the runtime graphic pages.Area– Allows the use of the “area” field associated with Power Operation project users. It can be configured on a per application level including: Power Operation reporting, Reporting (PME), WebReach, and Dashboards, and provides the ability to limit the use of SSO operations to specific areas.PrivLevel– Allows the use of the “privilege level” field associated with Power Operation project users. It can be configured on a per-application level including: Power Operation reporting, Reporting (PME), WebReach, Dashboards, and provides the ability to limit use of SSO operations to specific privileges.UseHTTPS– Default value:TRUE. Required in Power Monitoring Expert 2022PSEHostname– If you want to use Power Operation basic reports, use this parameter. This parameter specifies the IP address for the Power Operation Server.