Configuring projects for network segmentation
Power Operation can be configured to communicate with multiple network adapters in a network segmentation architecture. For security reasons, consider network segmentation for the following scenarios:
- Multiple Power Operation servers or clients are configured to run over a WAN or the Internet.
- Confirm that appropriate security precautions (such as a VPN) are used when connecting networks over a potentially public link (such as the Internet).
- An untrusted corporate network is connected to the control system network.
To configure a Power Operation project for network segmentation, follow these guidelines:
- Go to the AVEVA Knowledge & Support Center website for information on adding network addresses.
- Vijeo Citect 2015 Web Client Guide: Port-Forwarding / Address Forwarding (see Power Operation 2022Installation disc)
- Default port numbers