Creating a Category

You create a category when you want to organize your components in the Components pane or snippets in the Snippets pane.

For more information on categories, see Categories Overview.

To create a category:

  1. In Graphics Editor, in the Components pane or in the Snippets pane, right- click and then click New Category.
  2. In the New Component Category dialog box, type a name for the category.
  3. Click OK.

The new category is displayed as a tab in the Components pane or Snippets pane.