Importing a Snippets Category‌

You import a snippets category into the snippets library to be able to reuse the snippets between different projects.

For more information on categories, see Categories Overview.

To import a snippets category:

  1. In Graphics Editor, in the Snippets pane, right-click and then click Import.
  2. Select the .tgmlsnippetArchive file that contains the snippets you want to import.
  3. Click OK.

The imported snippets category is displayed as a tab in the Snippets pane.