Adding a Snippet
You add snippets to a graphic to add pre-programmed behaviors, such as colors changing according to the state of a point or numerically displayed values.
To add a Snippet:
- In Graphics Editor, in the Layers pane, select the layer where you want to add the snippet.
- In the Snippets pane, select the snippet category tab that contains the snippet you want to use.
- Select the snippet you want to add to the graphic.
- Drag the snippet to the work area or to a drawing object.
- On the Drawing toolbar, click Select.
- On the Options toolbar or in the Properties pane, adjust the appearance of the snippet.
- On the File menu, click Save.