Graphics Editor File Menu
Use the File menu to manage graphic files:
Command | Description |
---|---|
New | Opens a submenu where you can select if you want to create a graphic or a component. |
Open | Opens a submenu where you select a.tgml graphic file or an .ogc file. |
Save | Saves the graphic as a Power Operation object in the database. |
Save As | Opens a submenu where you select how the current graphic file is to be saved. When you use the Save As command to save a graphic as a file, the Power Operation link is broken. |
Import | Opens a dialog box where you can locate graphics files that you want to import into Graphics Editor. |
Export | Exports a graphics file to the selected location, under the name you enter, and in the file format you specify. |
Opens a submenu where you can make a number of print preferences for printing the active graphic or component. | |
Properties | Opens the document properties pane. For more information, see the Graphics Editor Properties Pane section. |
Settings | Opens a submenu from which you access user interface settings for Graphics Editor. |
Close | Closes the current design and the editor in which it is open. If you have several instances of the editor open simultaneously, only the current editor is closed. |
Exit | Exits all instances of the program. |