Session timeout
Use the session timeout settings to define the timeout behavior of the software web applications.
NOTE: You can enter a timeout value from 1 minute to 1440 minutes (1 day)
When a session timeout is configured, web application clients are logged out after a period of inactivity. The default timeout is 20 minutes. To restart or unlock the session you must enter the login credentials.
A session is considered inactive when none of the following actions are detected for the duration of the timeout period:
- Mouse movement
- Mouse clicks
- Keyboard activity
- Touch screen activity
NOTE: If you are integrating PO with EcoStruxure Building Operation, set the inactivity timeout in EBO to be higher than the value in PO.