Sepam event reading parameters
EventTable
This parameter defines the Sepam event table that the Sepam driver uses to collect alarms from a device. This allows two primaries to extract alarms from the same device. Valid values are 1 or 2.
Parameter type: integer
Default value: 1
Example:
[SEPAM40.MYCLUSTER.PORTO_1.DEVICE_A]
EventTable 2
EventIdle
This parameter defines the time that the driver will wait before requesting the next event from a Sepam device. It may be possible to reduce this value to increase the rate at which alarms can be retrieved from the device.
Parameter type: milliseconds
Default value: 500
Example:
[SEPAM40.MYCLUSTER.PORTO_1.DEVICE_A]
EventIdle 200