Default Genie Library

The genie library includes a number of general genies for objects such as motors and pumps. There are also genies that are specific to Power Operation. These genies use a particular naming convention, which is described in the table below. In the Power Operation library, each genie name begins with “pls,” and is followed by a description of the type of genie according to this table:

first

second

third

fourth

pls

indicates Power Operation library

alarm = alarm

base = primitive genies

1 = small

ansi = ANSI style

cb = circuit breaker

2 = large

display = equipment details

sw = switchgear

 

gen = generic

cmd = control genies

 

iec = IEC style

eq = equipment (devices)

 

style = navigation

 

 

 

 

 

Additionally, the actual genies have abbreviated names. When you highlight a genie name, the abbreviation displays above the top row of genie icons.

The following tables list and define the individual genies in each of the Power Operation libraries.

PLS_ALARM

This library includes genies that provide functionality to alarm displays.

Genie Abbreviation

Description

Field

data portion of an alarm row

Row

a genie with a collection of fields

Selector

for column resizing

Setpoint

a setpoint row

PLS_ANSI_BASE_1 / PLS_ANSI_BASE_2

These libraries include a variety of base symbols used to created genies for ANSI equipment.

1 = small size
2 = large size

Genie Abbreviation

Description

sl_battery_gen

single-cell battery

sl_battery_multi

multiple-cell battery

sl_capacitor

capacitor

sl_capacitor_vari

variable capacitor

SL_Closed_HV

closed circuit breaker position

sl_closed_knife

closed knife switch

sl_closed_lv

closed low-voltage circuit breaker

sl_conductive_path_1

conductive path 1

sl_conductive_path_2

conductive path 2

sl_conductive_path_3

conductive path 3

sl_conductor_junction

conductor junction

sl_contact_nc_closed

contact break, closed

sl_contact_nc_open

contact break, open

sl_contact_no_closed

contact make, closed

sl_contact_no_open

contact make, open

sl_contact_term

contact terminal

sl_ct

current transformer

sl_in_cb_rack

incoming, circuit breaker racked out, plug

SL_In_Rack

incoming, circuit breaker racked out, socket

sl_in_sw_head

incoming switch head

sl_inductor

inductor

sl_inductor_adjust

adjustable inductor

sl_inductor_gen

general inductor

sl_inductor_magcore

magnetic core inductor

sl_inductor_vari

variable inductor

sl_open

open symbol

sl_open_fuse_sw

open isolating fuse-switch

SL_Open_HV

open high-voltage circuit breaker

sl_open_knife

open knife-type switch

SL_Open_LV

open low-voltage circuit breaker

sl_out_cb_rack

outgoing, circuit breaker racked out, plug

SL_Out_Rack

outgoing, circuit breaker racked out, socket

sl_pb_break

push-button, break

sl_pb_make

push-button, make

sl_pb_term

push-button, terminal

sl_pt

potential transformer

sl_relay

relay

sl_resistor

resistor

sl_resistor_adjust

adjustable resistor

sl_resistor_vari

variable resistor

sl_separable_con_closed

separable connector, closed

sl_separable_con_open

separable connector, open

sl_separable_con_plug

separable connector plug

sl_separable_con_socket

separable connector socket

PLS_ANSI_CB_1 / PLS_ANSI_CB_2

These libraries include genies for ANSI-type high-voltage and low-voltage drawout circuit breakers.

1 = small size
2 = large size

Additional definitions:

bus

=

busway

cb

=

circuit breaker

 

 

 

hv

=

high voltage

lv

=

low voltage

 

 

 

dr

=

drawout

nd

=

non-drawout

 

 

 

fd

=

earth at bottom (feeder)

inc

=

earth at top (incomer)

nes

=

no earth

 

 

 

nc

=

not remote control

c

=

remote control

 

Genie Abbreviation

Description

hv_cb_bus_dr_c

high-voltage drawout circuit breaker, remote control

hv_cb_bus_dr_nc

high-voltage drawout circuit breaker, not remote

hv_cb_bus_nd_c

high-voltage non-drawout circuit breaker, not remote

hv_cb_bus_nd_nc

high-voltage non-drawout circuit breaker, not remote

hv_cb_fd_dr_c

high-voltage, drawout circuit breaker, remote control, with earth at bottom

hv_cb_fd_dr_nc

high-voltage, drawout circuit breaker, no remote control, with earth at bottom

hv_cb_fd_nd_c

high-voltage, non-drawout circuit breaker, remote control, with earth at bottom

hv_cb_fd_nd_nc

high-voltage, non-drawout circuit breaker, no remote control, with earth at bottom

hv_cb_inc_dr_c

high-voltage, drawout circuit breaker, remote control, with earth at top

hv_cb_inc_dr_nc

high-voltage, drawout circuit breaker, no remote control, with earth at top

hv_cb_inc_nd_c

high-voltage, non-drawout circuit breaker, remote control, with earth at top

hv_cb_inc_nd_nc

high-voltage, non-drawout circuit breaker, no remote control, with earth at top

hv_cb_nes_dr_c

high-voltage drawout circuit breaker, remote control, no earth

hv_cb_nes_dr_nc

high-voltage drawout circuit breaker, no remote control, no earth

hv_cb_nes_nd_c

high-voltage non-drawout circuit breaker, remote control, no earth

hv_cb_nes_nd_nc

high-voltage non-drawout circuit breaker, no remote control, no earth

lv_cb_bus_dr_c

low-voltage drawout circuit breaker, remote control, busbar-type with earth at bottom

lv_cb_bus_dr_nc

low-voltage drawout circuit breaker, no remote control, busbar-type with earth at bottom

lv_cb_bus_nd_c

low-voltage non-drawout circuit breaker, remote control, busbar-type with earth at bottom

lv_cb_bus_nd_nc

low-voltage non-drawout circuit breaker, no remote control, busbar-type with earth at bottom

lv_cb_fd_dr_c

low-voltage drawout circuit breaker, remote control, earth on load side (bottom of drawing)

lv_cb_fd_dr_nc

low-voltage drawout circuit breaker, no remote control, earth on load side (bottom of drawing)

lv_cb_fd_nd_c

low-voltage non-drawout circuit breaker, remote control, earth on load side (bottom of drawing)

lv_cb_fd_nd_nc

low-voltage non-drawout circuit breaker, no remote control, earth on load side (bottom of drawing)

lv_cb_inc_dr_c

low-voltage drawout circuit breaker, remote control, earth on feeder (top of drawing)

lv_cb_inc_dr_nc

low-voltage drawout circuit breaker, no remote control, earth on feeder (top of drawing)

lv_cb_inc_nd_c

low-voltage non-drawout circuit breaker, remote control, earth on feeder (top of drawing)

lv_cb_inc_nd_nc

low-voltage non-drawout circuit breaker, no remote control, earth on feeder (top of drawing)

lv_cb_nes_dr_c

low voltage drawout circuit breaker, no earth, remote control

lv_cb_nes_dr_nc

low voltage drawout circuit breaker, no earth, no remote control

lv_cb_nes_nd_c

low voltage non-drawout circuit breaker, no earth, remote control

lb_cb_nes_nd_nc

low voltage non-drawout circuit breaker, no earth, no remote control

PLS_ANSI_SW_1 / PLS_ANSI_SW_2

These libraries include ANSI-style switches:

1 = small size
2 = large size

Genie Abbreviation

Description

sw_fused

switch: feeder, fused

sw_fused_isolated

switch: feeder, fused, isolated

sw_general

switch: feeder, general

sw_knife

switch: knife type

PLS_DISPLAY

This library includes two genies that provide data row items for equipment.

Genie Abbreviation

Description

equiplistitem

data row for the equipment tag list

EquipValueItem

data row for the equipment popup

PLS_GEN_BASE_1 / PLS_GEN_BASE_2

These libraries include a variety of "parts" related to generators, motors, and transformers.

Genie Abbreviation

Description

chassis_ground

chassis ground

Dev_Base

device base

es_inc

earth switch, incomer

es_out

earth switch, feeder

Gen_1

generator, option 1

Gen_2

generator, option 2

gen_AC

generator: AC

gen_DC

generator: DC

genset

engine-generator

ground

ground

Motor_1

motor, option 1

Motor_2

motor, option 2

motor_ac

motor: AC

motor_dc

motor: DC

motor_synch

motor: synchronous

SL_Base

circuit breaker base symbol

sl_br_in

circuit breaker line in, non-drawout

sl_br_out

circuit breaker line out, non-drawout

SL_Bustie

bus tie

SL_CommLoss

comms loss

SL_Discrepancy

position discrepancy

sl_harmonic_filter_1

harmonic filter 1

sl_harmonic_filter_2

harmonic filter 2

SL_In

incoming bus

SL_Local

local, rather than remote control

SL_Out

feeder

SL_Tripped

tripped

Test_CB_Control

health test for the circuit breaker control

transformer_1_in

transformer 1: general, on-line

transformer_1_in_y

transformer 1: star (wye), on-line

transformer_1_out

transformer 1: general, off-line

transformer_1_out_d

transformer 1: delta, off-line

transformer_1_out_y

transformer 1: star (wye), off-line

transformer_2_in

transformer 2: general, on-line

transformer_2_in_Y

transformer 2: star (wye), on-line

transformer_2_out

transformer 2: general, off-line

transformer_2_out_D

transformer 2: delta, off-line

transformer_2_out_Y

transformer 2: star (wye), off-line (no 2 IN D? or 1 IN D?)

PLS_GEN_CMD_1 / PLS_GEN_CMD_2

These libraries include genies that control display of popups and values:

1 = small size
2 = large size

Genie Abbreviation

Description

CmdDetail

provides access to the equipment detail popup

cmddetail_meter

provides access to the meter detail popup

Control

control in a circuit breaker

value

value section of a circuit breaker

value_meter

value section of a meter

PLS_GEN_EQ_1 / PLS_GEN_EQ_2

These libraries include the general equipment used to make up generators, motors, and transformers:

1 = small size
2 = large size

Genie Abbreviation

Description

busbar_horz

horizontal busbar

busbar_vert

vertical busbar

gen_ac

generator: AC

gen_dc

generator: DC

gen_nd_1

generator 1: no current designation

gen_nd_2

generator 2: no current designation

mot_ac

motor: AC

mot_dc

motor: DC

mot_nd_1

motor 1: no current designation

mot_nd_2

motor 2: no current designation

mot_syn

motor, synchronous

trans_nd_1

transformer 1: no connection designation

trans_nd_2

transformer 2: no connection designation

trans_sd_1

transformer 1: star-delta (wye-delta)

trans_sd_2

transformer 2: star delta (wye-delta)

trans_ss_1

transformer 1: star-star (wye-wye)

trans_ss_2

transformer 2: star-star (wye-wye)

PLS_IEC_BASE_1 / PLS_IEC_BASE_2

These libraries include a variety of symbols for IEC equipment:

1 = small size
2 = large size

Genie Abbreviation

Description

sl_cap_bank_tuned_3

capacitor bank 3: tuned

sl_cap_bank_tuned_4

capacitor bank 4: tuned

sl_capacitor

capacitor

sl_capacitor_vari

capacitor, variable

sl_closed

closed switch

sl_contact_nc

contact break

sl_ct

contact

sl_fuse_1

fuse, option 1

sl_fuse_2

fuse, option 2

SL_Head

head

sl_head_2

head

sl_in_cb_rack

incoming, circuit breaker when racked out, plug

SL_In_Rack

incoming, circuit breaker when racked out, socket

sl_in_sw_hd_isol

incoming, switch head, isolated

sl_in_sw_head

incoming, switch head

sl_inductor

inductor

sl_inductor_adjust

inductor, adjustable

SL_Open

open

sl_out_cb_rack

feeder, circuit breaker when racked out, plug

SL_Out_Rack

feeder, circuit breaker when racked out, socket

sl_resistor

resistor

sl_resistor_adjust

resistor with adjustable contact

sl_resistor_vari

resistor, variable

sl_sw_static_1

static switch 1

sl_sw_static_2

static switch 2

PLS_IEC_CB_1 / PLS_IEC_CB_2

These libraries include high-voltage drawout circuit breakers:

1 = small size
2 = large size

Genie Abbreviation

Description

hv_cb_bus_dr_c

high-voltage drawout circuit breaker, remote control

hv_cb_bus_dr_nc

high-voltage drawout circuit breaker, no remote control

hv_cb_bus_nd_c

high-voltage non-drawout circuit breaker, remote control

hv_cb_bus_nd_nc

high-voltage non-drawout circuit breaker, no remote control

hv_cb_fd_dr_c

high-voltage, drawout circuit breaker, remote control, earth at bottom

hv_cb_fd_dr_nc

high-voltage, drawout circuit breaker, no remote control, earth at bottom

hv_cb_fd_nd_c

high-voltage, non-drawout circuit breaker, remote control, earth at bottom

hv_cb_fd_nd_nc

high-voltage, non-drawout circuit breaker, no remote control, earth at bottom

hv_cb_inc_dr_c

high-voltage, drawout circuit breaker, remote control, earth at top

hv_cb_inc_dr_nc

high-voltage, drawout circuit breaker, no remote control, earth at top

hv_cb_inc_nd_c

high-voltage, non-drawout circuit breaker, remote control, earth at top

hv_cb_inc_nd_nc

high-voltage, non-drawout circuit breaker, no remote control, earth at top

hv_cb_nes_dr_c

high-voltage drawout circuit breaker, remote control, no earth

hv_cb_nes_dr_nc

high-voltage drawout circuit breaker, no remote control, no earth

hv_cb_nes_nd_c

high-voltage non-drawout circuit breaker, remote control, no earth

hv_cb_nes_nd_nc

high-voltage non-drawout circuit breaker, no remote control, no earth

PLS_IEC_SW_1 / PLS_IEC_SW_2

These libraries include IEC-style switches:

1 = small size
2 = large size

Genie Abbreviation

Description

sw_general

general switch

sw_isolated

isolated switch

PLS_METER

This library includes meter symbols.

Genie Abbreviation

Description

circuit monitor

Power Operation circuit monitor

egx

Power Operation EGX

generic_meter

generic meter

ion_7650

ION 7650 meter

micrologic

all Mircologic meters

power_meter

Power Operation power meter

quantum

Power Operation Quantum

sepam

all Sepam meters

ITEM1

This library includes miscellaneous symbols.

Genie Abbreviation

Description

Item1

value type and units block for a circuit breaker

Item2

value type and units block for a circuit breaker

tab1

menu tab

Tab2

menu tab