Alarm to Incident Mapping
The following table shows the mapping of alarm types to Incidents:
Incident Category | Incident Type | Alarm Types |
---|---|---|
Power Quality | Interruption | Interruption |
Over Voltage | Over Voltage | |
Under Voltage | Under Voltage | |
Unclassified Disturbance | Unclassified Disturbance | |
Sag | Sag (Voltage) | |
Swell | Swell (Voltage) | |
Transient | Transient | |
Flicker | Flicker | |
Frequency Variation | Frequency Variation | |
Harmonics | Harmonics | |
Harmonics (Current) | ||
Harmonics (Power) | ||
Harmonics (Voltage) | ||
Unbalance | Unbalance | |
Unbalance (Current) | ||
Unbalance (Voltage) | ||
Diagnostics | Communication Status | Communication Status |
Device Status | Device Status | |
System Status | System Status | |
Energy Management | Air | Air |
Demand | Demand | |
Electricity | Electricity | |
Gas | Gas | |
Power Factor | Power Factor | |
Steam | Steam | |
Water | Water | |
Asset Monitoring | Arc Flash | Arc Flash |
Protection | Protection | |
Backup Power | Backup Power | |
Current Monitor | Over Current | |
Sag (Current) | ||
Swell (Current) | ||
Under Current | ||
Thermal Monitor | Thermal Monitor | |
General | Clutter | General Event |
Clock / Time | ||
Device Settings | ||
Unassociated Dropout | ||
General Setpoints | General Setpoint |