Busbar
A busbar is a metallic strip or bar (typically copper, brass or aluminium) that conducts electricity within a switchboard, distribution board, substation, battery bank, or other electrical apparatus to make a common connection between several circuits in a system.
Busbar has only one bind property; BusColor.
The graphic representation of the default position and the bind property is shown in the below table:
| Bind Property | Description | Graphic |
|---|---|---|
| NA | Busbar is in default position. |
|
| BusColor | Sets the bus color. |
|