Generator

A generator is a device that converts mechanical energy into electrical energy for use in an external circuit.

The different types of generators that are supported in the Power Operation are:

  • Gen_AC
  • Gen_DC
  • Gen_nd_1
  • Gen_nd_2

Generator has only one bind property; BusColor.

The graphic representation of the default position and the bind property is shown in the below table:

Bind Property Description Graphic
NA Generator is in default position.
BusColor Sets the bus color.
  • TopBusColor
  • IsTripped
  • IsClosed
  • RkdPos
  • BottomBusColor
  • EarthSwitchClosed