LiveView Power Flow Summary

This summary displays a power flow summary for your system devices. Use the information from this table to help optimize the system's power flow.

After opening the power flow summary template, you set the update interval for this summary. You can also add or remove devices from the summary.

Make your selections, and click Display Table.

The power flow summary provides this data:

  • real power (kW)
  • reactive power (kVAR)
  • apparent power (kVA)
  • demand average (kW)
  • demand peak (kW)
  • predicted demand (kW)