Menus and Display Pages

Use Menus and Display Pages to add top-level menus that display in the runtime human-machine interface (HMI). The HMI is the view that users see. You can also define the default runtime page that will display on a monitor.

To add menus and landing pages:

  1. Under HMI Menus, click the top-level menu items that you want to include in the HMI.

    NOTE: You can add more menu levels in the Power Operation Studio Menu Configuration page: Visualization > Menu Configuration.

  2. (Optional)  If you have multiple monitors in your system:
    1. Under Monitors, enter the number (up to 8) of monitors in the Total Monitors field. You can also click the plus and minus buttons to increase or reduce the number.
    2. Under Runtime Landing Page, the corresponding number of monitors are enabled.
    3. For each monitor, select landing page you want to see when this monitor views Power Operation
  3. Select Next.

For more information on Power Operation menu configuration, see Power Operation Runtime menus.