Default port numbers

Each server component has a unique default port assigned to it. This default port may only be used with that type of server. However, application engineers may choose ports other than the defaults, depending on the design of the project. Non-default ports need to also be added to the firewall exceptions.

Which ports are required for a specific installation depends on the Power Monitoring Expert system configuration and the monitoring devices used.

If Power Operation alarm, trend, report and I/O servers are created using non-default ports, create those ports exceptions.

Service Default port Description
Alarm Server (Citect) 5482

Database port for alarms.

Alarm Server (Citect) 2080 Synchronization between redundant Citect alarm server components.
Application Server 23103 Web services used by Basic Reports and Live View.
Client (Citect) 2074 Cicode (custom script) debugging.
Client access or ActiveX web client 5500-5509 Ports used for thick control client and ActiveX web client to communicate to server.
CTAPI (Citect) 2073 Used by Power Operation components to interact with Citect server processes.
CTAPI (encrypted connections) 3073 Used by Power Operation components to interact with Citect server processes.
Database 5432 Used to connect to PostreSQL Database Engine.
Event Notification 23104 Synchronization between redundant Power Operation notification servers.
FTP, IDC 21 Page downloads for IDC, Internet Display Server/Client communications.
I/O Server (Citect) 2082 Publish and subscribe I/O server communications.
ODBC 20222 Open Database Connnectivity server.
OPC UA 48031 OPC Unified Architecture communication
Report Server (Citect) 2084 Report server communications.
Platform Server 23201 Services for communications with the Service Layer Platform Server.
System services process 2087 Runtime running as a service.
Time synchronization port 2088 To enable time synchronization.
Trends Server (Citect) 2085 Synchronization between redundant Citect trend server communications.
Web Server 443 WebHMI application. Access to page and document content, diagrams, and all system data.
Service Layer 23200 Services for communications with the Service Layer Pso Web Service.

Default port numbers and associated server types

HTML5 Web Client

 

Thick Client

For information about the ports for Advanced Reporting and Dashboards, see Ports in the Power Monitoring Expert – IT Guide.