Web Client Access license

Power Operation Web Client Access licenses are optional components that allow operators to access the Power Operation system using an HTML5 web client. The alarms and waveform web functionality is mobile responsive. The Web Client Access license is only available with the 2020 version of the software and above.

An equal number of Web Client Access licenses must be purchased for each Server in your system.

The Web Client Access license uses a concurrent license model that enforces the number of simultaneous connections from remote machines. Unlike Power Monitoring Expert, it does not enforce the number of names of operators for the systems.

Licensing options

  • Web Client Access is licensed by the number of points/tags (the options are 500, 1500, 5000, 15000, and Unlimited).
  • Web Client Access licenses need to have at least the same point count as the Server that they are connected to.