Connected devices and protocols

Power Operation supports concurrent protocol communication; one Power Operation server can communicate using multiple protocols.

Power Operation 2024 supports the following protocols:

  • IEC 61850 Primary (sometimes called Master) Edition 2
  • DNP3 Primary
  • ION
  • Modbus Primary
  • IEC 60870-5-104 Primary
  • KNX
  • SNMP
  • BACnet/IP

Power Operation supports the following Open Data Exchanges:

  • OPC UA 1.01 (Client and Server)
  • OPC DA version 2, version 2.05a (Client and Server)
  • OPC AE version 1 (Server)

Go to the AVEVA Knowledge & Support Center website for information on Plant SCADA.

Topics in this section: