Power SCADA Anywhere component

Power SCADA Anywhere is a legacy solution that was substituted with the HTML5 PO 2021 web client.

It is an optional component and is an HTML5 streaming application that allows for the visualization of the Power Operation Runtime from any HTML5-compliant browser (Edge, Chrome, Firefox, etc.) by streaming a remote desktop application from a Client Access.

Power SCADA Anywhere 2023 is compatible with:

  • EPO 2024
  • EPO 2022
  • EPO 2021
  • PSO 2020 R2
  • PSO 2020
  • PSO 9.0

Upgrade considerations

Upgrade considerations from version 1.0 and 1.1 to version 1.2:

  • License upgrade is not required if you are upgrading from Anywhere 1.x.
  • For instructions on upgrading Power SCADA Anywhere Server, refer to the "Upgrading to a New Version" section of the Power SCADA Anywhere Server Installation and Configuration Guide.

Supported operating systems

Power SCADA Anywhere Server 1.2 software has been tested to run on:

  • Microsoft Windows Server 2019
  • Microsoft Windows Server 2016
  • Microsoft Windows Server 2012 R2
  • Microsoft Windows Server 2012
  • Microsoft Windows Server 2008 R2 SP1

Host requirements

Power SCADA Anywhere host requirements for disk, CPU and RAM are negligible.

Power SCADA Anywhere host must have CPU with SSE2 instruction set support.

Browser requirements

Power SCADA Anywhere is supported in the following browsers:

  • Internet Explorer 11
  • Edge
  • Chrome
  • Safari

When using the Power SCADA Anywhere client, we are assuming that the various components listed below are integrated into a runtime experience that is being used in a Client Access such as Power SCADA thick client graphics pages, including 1-line diagram/engine built with Citect graphics:

  • PME reports, PME dashboards, and PME WebReach Diagrams
  • Power Operation Basic Reports
  • LiveView (Power SCADA Real Time Tables implementation)
  • Event Notification Module (configuration tools)

When these components are integrated into a runtime that is streamed using Power SCADA Anywhere, all HTML5 client browsers listed previous are supported.

Multiple instances of Power SCADA Anywhere can be opened at the same time in a web browser.

Windows Active Directory support

Power SCADA Anywhere users can only be managed through Windows Active Directory. The machine hosting Power SCADA Anywhere must be installed on a machine that is part of a Windows domain.

Licensing options

Each Power SCADA Anywhere license allows up to 5 concurrent connections to the runtime through HTML5 web browsers. For more information on licensing, see License keys.

Design considerations

  • Power SCADA Anywhere requires an equal number of Power Operation Client Access to be licensed.
  • Power SCADA Anywhere requires a domain to use Windows Remote Desktop licenses.
    • The Power SCADA Anywhere host cannot be installed on a domain controller.

  • Since Power SCADA Anywhere uses Windows remote desktop connections, it requires an equal number of Windows Remote Desktop Services (RDS) client access licenses to be purchased.