Server requirements for distributed PostgreSQL
PostgreSQL is an open source object-relational database system added to Power Operation to store waveform and alarm analytics information (e.g. probable cause, etc.).
PostgreSQL components can be either:
- Installed on the same machine as the Power Operation Server. (This is the default behavior.)
- Installed in a distributed architecture either on Windows OS or Linux OS.
CPU, RAM, and disk requirements
If installing PostgreSQL on a separate machine from the Power Operation Server, you will need the following for a distributed PostgreSQL environment:
- Disk storage: Minimum 80 GB free disk space
- CPU: Single core with minimum 2GHZ
- RAM: 4 GB
NOTE: The product team has validated the distributed Linux architecture with RHEL 8 - Red Hat Enterprise Linux 8. If you are considering other Linux variants, we recommend to refer to PostreSQL's supported Linux versions.