Supported SQL Server versions

Power Operation with Advanced Reporting and Dashboards requires a Microsoft SQL Server database. Power Operation with Advanced Reporting and Dashboards supports the following SQL Server versions: 

  • SQL Server 2019 Express/Standard/Enterprise/Business Intelligence
  • SQL Server 2017 Express/Standard/Enterprise/Business Intelligence
  • SQL Server 2016 Express/Standard/Enterprise/Business Intelligence
  • SQL Server 2014 Express/Standard/Enterprise/Business Intelligence
  • SQL Server 2012 Express/Standard/Enterprise/Business Intelligence, SP2

NOTE: Power Operation 2024 without Advanced Reporting and Dashboards does NOT require a SQL Server database.

Power Operation with Advanced Reporting and Dashboards installation media includes SQL Server 2019 Express that can be used with Advanced Reporting.