Integrating with Advanced Reporting and Dashboards
The Advanced Reporting and Dashboards Module offers a broad array of reports, dashboard visualizations, and customizable report subscriptions.
- Power Monitoring Expert Reporting
- Best in class reporting with more than 30 default reports, including Power Quality reports
- Reports that can be triggered manually, scheduled, or event-triggered
- Save reports as PDF, HTML, or CSV
- Power Monitoring Expert Dashboards- End user configurable dashboard view of historical data
- Ability to embed external web content in a dashboard
- Kiosk views to let teams see KPI Energy values that are relevant to them
 
- Power Monitoring Expert WebReach diagrams- Diagram-based view of real time device data
 
- Provide historical data to Power Advisor for analytics
When Power Operation and Power Monitoring Expert are integrated, historical applications from PME (Reports and Dashboards) are integrated into the Power Operation runtime. WebReach diagrams are also frequently integrated with Power Operation resulting in a seamless end user experience.
The following table lists how components are used in combined solution:
| Real time information (graphics, tables, trends) | Alarms | ENM | Waveforms | Historical reports and dashboards | OPC UA and SMNP | |
|---|---|---|---|---|---|---|
| Power Operation | Enabled animated 1-line, LiveView, Power Operation real time and historical trends | Enabled | Enabled | Enabled used for sequence of events analysis | Basic Reports Enabled when large data acquisition such as 1 minute logging is required by customer | Enabled built-in drivers within Power Operation used | 
| Power Monitoring Expert | Disabled Vista, real time and historical trends | Disabled | Disabled not configured with PME | Enabled used by PME PQ reports | Enabled PME Web Reports and Dashboards integrated into Power Operation runtime | N/A | 
NOTE: Power Operation with Power Monitoring Expert must be the same product version to be integrated.