Core components selection

The installer provides a list of options to help you select the appropriate components during installation. The options are described here.

Client Runtime

Selects Client Runtime, Deployment Client, and OPC UA Server drivers (optional) for installation. It is an installation that installs the runtime components for a client. This installation includes Aveva runtime client only installer, EcoStruxure™Power Operation Notification DLL, and License module.

Select this option if this is an installation of Power Operation that will act as a client.

Server Runtime

Selects Server Runtime, Deployment Client, and OPC UA Server drivers (optional) for installation. It is an installation that installs the Aveva runtime server. It also includes the following components: Legacy AOL, App Configuration utility, Waveform Extractor, Core Services, Web Services, Postgres, WebHMI, Legacy Web applications, Event Notification, Power Operation Licese Configuration tool, and the License module.

Select this option if this is an installation of Power Operation that will act as a server to service many client installations.

Configuration and Development Environment

Installs the design-time configuration environment. Users who have sufficient security privileges can select add-on components such as Power Operation Profile Editor and Power Operation EWS Server. The configuration tools include: Power Operation Studio, Graphics Editor, Template Editor, TGML Update Utility, IO Device Manager, Rapid Deployment Wizard, and Power Operation Migration Tool.

Deployment Client

Installs the Deployment Client component, which allows projects to be deployed to this machine remotely. This option is selected automatically if you select the Client Runtime, Server Runtime, or OPC UA Server option.

Deployment Server

Installs the Deployment Server component, which allows projects to be administered, versioned, and deployed to other remote Deployment Client machines from this machine. The server can roll out project changes to the various computers in your project. This option is disabled if you select the Client Runtime or Server Runtime option.

OPC UA Server

Installs the OPC UA server component on the same machine as Power Operation. Deployment Client installation is mandatory for OPC UA Server. It is installed and hosted on the Power Operation Server. This enables the Power Operation system to send and receive data from a third-party application via OPC UA.