Installing
You can install Power Operation with Advanced Reporting and Dashboards as a new product only. You must uninstall previous versions before installing v2024. Power Operation does not support different versions running side-by-side. If you are upgrading from an earlier version of Power Operation, back up your existing project files. These files include LiveView templates; reporting configurations (such as email addresses); and Profile Editor custom tags, device types, profiles, and units (in the Program Data folder). Remove existing Power Operation License Configuration Tool installations before installing the new version.
Before proceeding with the installation of Power Operation with Advanced Reporting and Dashboards and optional components, refer to Before installing for detailed installation prerequisite information.
NOTE: Renaming your machine after installation will cause the runtime to fail.