Preparing servers

The software Installer performs several of the setup and configuration tasks during installation to ensure that the prerequisites for your Power Operation with Advanced Reporting and Dashboards system are met. Complete the following before proceeding with the installation.

Updating the operating system

warning

potential compromise of System availability, integrity, and confidentiality

Apply the latest updates and hotfixes to your Operating System and software.

Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.

Run the Windows Update service to install the latest security patches and hotfixes from Microsoft.

Advanced Reporting and Dashboards Module Server

For more information, on server requirements and preparation, see the Advanced Reporting and Dashboards component.